CERTIFICATE OF COMPLIANCE
To whom it may concern,
This document certifies that to the best of Eaton’s knowledge the catalog part number stated below is in conformity with Directive 2011/65/EU of the European Parliament and of the Council of 8 June 2011 on the restriction of the use of six specific substances at maximum concentration values tolerated by weight in homogeneous materials; Lead (0,1 %); Mercury (0,1 %); Cadmium (0,01 %); Hexavalent chromium (0,1 %); Polybrominated biphenyls (PBB) (0,1 %); Polybrominated diphenyl ethers (PBDE) (0,1 %) in electrical and electronic equipment, according to Annex II of EC Directive 2011/65/EU, and amendment to Annex II (EU) 2015/863 of 31 March 2015 to Directive 2011/65/EU of the European Parliament and of the Council as regards of the list of four restricted substances at maximum concentration values tolerated by weight in homogeneous materials, Bis(2-ethylhexyl) phthalate (DEHP) (0,1 %); Butyl benzyl phthalate (BBP) (0,1 %); Dibutyl phthalate (DBP) (0,1 %); Diisobutyl phthalate (DIBP) (0,1 %). Therefore, the stated catalog part number reference in this document is deemed compliant in accord with definitions given in this directive.
Catalog Number: 0402ESDA-MLP7
Date Code: 13CH04
Date Code: 13CH04